Kollmorgen UDFBs

A KollmorgenUDFB"User Defined Function Block" UDFB can be used as a sub-function block in another program of the application. It is described using FBD, LD, ST or IL language. Input / output parameters of a UDFB (as well as private variables) are declared in the variable editor as local variables of the UDFB is a pre-defined function block created by Kollmorgen to simplify certain tasks or demonstrate a particular function. A Kollmorgen UDFB"User Defined Function Block" UDFB can be used as a sub-function block in another program of the application. It is described using FBD, LD, ST or IL language. Input / output parameters of a UDFB (as well as private variables) are declared in the variable editor as local variables of the UDFB must be instantiated before it may be used. The code inside a Kollmorgen UDFB can be modified by creating an unlocked copy in the subprogram section in the project tree..

Name  Description 
FB_AKDFltRpt  Outputs AKD fault information
FB_AxisPlsPosModulo  Used for any position of a modulo axis in both directions
FB_AxisPlsPosNoModulo  Used for any position of a non-modulo axis in both directions
FB_Cylinder  Control a cylinder and the Limit Switches.
FB_ElapseTime  Keeps track of the time that a Boolean input variable is on.
FB_FirstOrderDigitalFilter  Filter an Analog signal.
FB_PWDutyOutput  Converts an input range to a duty cycle percentage
FB_S700FltRpt  Outputs S700"Servostar 700 drive" See Servo Drive in Glossary drive fault Information
FB_ScaleInput  Scale DINT to LREAL
FB_ScaleOutput  Scale DINT to LREAL
FB_TemperaturePID  Provides PID"Proportional-Integral-Derivative" A PID controller is a generic control-loop feedback mechanism widely used in industrial control systems. An "error" occurs when an event or a disturbance triggers off a change in the process variable. A PID controller attempts to correct the error between a measured process variable and a desired setpoint by calculating and then outputting a corrective action that can adjust the process accordingly temperature control with auto tuning
MCFB_AKDFault Outputs AKD drive fault Information.
MCFB_AKDFaultLookup String message of the corresponding AKD drive fault number
MCFB_GearedWebTension Facilitates dancer and tension control in an electronic geared master/slave machine design
MCFB_Jog  Jog an axis in the selected direction at a defined speed
MCFB_StepAbsolute  Performs a static homing function by setting Actual Position to the position of an absolute encoder
MCFB_StepAbsSwitch  Performs a homing function by searching for an absolute positioned external physical switch
MCFB_StepAbsSwitchFastInput  Performs a homing function by searching for an absolute positioned external physical switch
MCFB_StepBlock  Performs homing against a physical object, mechanically blocking the movement
MCFB_StepLimitSwitch  Performs a single-axis home to a limit switch
MCFB_StepLimitSwitchFastInput  Performs a homing function by searching for an external physical switch
MCFB_StepRefPulse  Performs homing by searching for Zero pulse, Marker, or reference pulse in encoder
MLFB_HomeFindHomeFastInput  Performs a single-axis home to a limit switch connected to a High Speed Input
MLFB_HomeFindHomeFastInputModulo  Performs a single-axis home to a limit switch connected to a High Speed Input
MLFB_HomeFindHomeInput  Fast HomingThe Homing procedure allows, based on a position measurement, to set a position offset to the motor in order to ensure it is physically at the home position to a home switch
MLFB_HomeFindHomeInputThenZeroAngle  Fast Homing to a home switch + Zero angle
MLFB_HomeFindLimitFastInput  Homing to a limit switch
MLFB_HomeFindLimitFastInputModulo  Homing to a limit switch: Modulo mode
MLFB_HomeFindLimitInput  Homing to a limit switch
MLFB_HomeFindLimitInputThenZeroAngle  Homing to a limit switch + Zero angle
MLFB_HomeFindZeroAngle  Homing to a zero-angle reference
MLFB_HomeMoveUntilPosErrExceeded  Homing until the position error is exceeded
MLFB_HomeMoveUntilPosErrExceededThenZeroAngle  Homing until the position error is exceeded + Zero angle
MLFB_HomeUsingCurrentPosition  Homing using the current position
MLFB_Jog  Jog in a selected direction at a defined speed
MLFB_PlsPosFw  Forward position range indicator
MLFB_PlsPosFwBw  Forward/Backward position range indicator
MLFB_PlsTimeFw  Forward/Backward position/time range indicator
PipeNetwork_FFLD  Used to call the PNCode function block in FFLD POUs
ProfilesCode_FFLD  Used to call the ProfilesCode function block in FFLD POUs

Table 10-50: List of System Kollmorgen UDFBs

How to create an instance

An instance of the UDFB has now been created in Subprograms.


  • You cannot create the instance of the UDFB directly from the dictionary or from the PLC Editor.

Working with Kollmorgen UDFBs

By default all Kollmorgen UDFBs are protected, meaning they may not be modified or renamed. When a Kollmorgen UDFB is dropped into an instance it is not editable. There are two solutions to make it editable:

  • Right click on a Kollmorgen UDFB that has been dropped into an instance (in Subprograms) and select Unlock. This creates an unlocked version of the UDFB with the name "U<sequence number><UDFB name>".

  • Instead of dropping a Kollmorgen UDFB into an instance, right click on the UDFB and select Create unlocked copy in Subprograms. This creates an unlocked instance of the UDFB with the name "U<sequence number><Kollmorgen UDFB name>".

Once a Kollmorgen UDFB has been unlocked it may be renamed and exported by right-clicking on the UDFB. Renamed UDFBs must have unique names. Importing a saved UDFB will increment the UDFB's name.


  • In order for a UDFB to modify a structure or array based on the output, you must first define it as an input. The input is automatically set as an INOUT parameter. This is because OUTs are strictly simple types.

 


Stay Connected with Kollmorgen

Copyright © 2018 Kollmorgen